The Frasnacht water treatment plant relies on analytical panels from Endress+Hauser to monitor the drinking water treatment process. The panels are clearly laid out, easy to use and extremely reliable – and apart from an annual service by Endress+Hauser service technicians, they’re completely maintenance-free.
Inside view of the water facility in Frasnacht, Switzerland.
Benefits
Accurate, stable and reproducible measured values guarantee maximum drinking water quality.
Trouble-free operation:The purified water panel has provided reliable measurements for almost two years without a hitch.
Easy to use:The measuring points are compact and laid out clearly on a panel. The measurements and calibrations of all parameters run together in one transmitter.
Completely hassle-free: Maintenance required only once a year by Endress+Hauser Service.
I can summarize my experience of the panel in three words: Fault-free, maintenance-free, perfect.
Rolf Bügler, Water Supervisor
Regionale Wasserversorgung St. Gallen
The Challenge
Several critical parameters are monitored continuously in the freshly extracted raw water as well as the purified water. Measurement results must be reliable, as the water supervisor will intervene in the water treatment process only if the measured values indicate that this is necessary. “We expect a measuring point to deliver accurate, stable and reproducible values, to run reliably and be easy to operate”, the water supervisor at the water treatment plant says.
Our solution
An analysis panel was deployed as a compact solution for the measurement of key parameters ranging from temperature, conductivity and pH to turbidity and SAC. The panel was custom-built to meet the customer’s exact requirements. It was supplied with all sensors and measuring devices already installed, thus ensuring straightforward and easy commissioning. Since then, two panels have been deployed for purified water monitoring and one for raw water monitoring.
Água, bebidas, laticínios e produtos químicos ou farmacêuticos precisam ser analisados todos os dias. Escolha o dispositivo mais adequado para as necessidades de seus processos com um portfólio abrangente.
Explore as soluções da Endress+Hauser para o segmento de tratamento de água para um monitoramento da qualidade da água potável econômico e confiável, hoje e no futuro.
Saiba mais sobre nossos sistemas robustos e completos de monitoramento de efluentes com manutenção inteligente que ajudam você a cumprir com seus limites legais e contratuais.
Você usa geradores de vapor para sua produção de alimentos ou bebidas? Descubra nossos painéis inteligente SWAS para o monitoramento confiável da qualidade da água na geração de vapor.
Descubra o monitoramento inteligente da Endress+Hauser para estações de tratamento de efluentes. Esteja em conformidade com valores limite com eficiência aprimorada com nossos sistemas de monitoramento completos, fáceis de usar e econômicos.
A Endress+Hauser está confiante em ajudá-lo a atingir suas metas operacionais em todo o ciclo da água, combinando um portfólio inovador de instrumentos de medição, serviços especializados e experiência no setor.
Regionale Wasserversorgung St. Gallen, Frasnacht, Switzerland
The Frasnacht water treatment plant is one of 17 water treatment plants on Lake Constance and forms part of the St. Gallen regional water supply system (RWSG). Opened in 1999, the plant has a daily capacity of 60,000 cubic meters of water and supplies 150,000 inhabitants in the region with drinking water.
Sua privacidade é muito importante
Usamos cookies para melhorar sua experiência de navegação, coletamos estatísticas para otimizar a funcionalidade do site e entregar anúncios e conteúdo personalizados.
Ao selecionar "Aceitar todos", você consente nosso uso de cookies.
Para mais detalhes, revise nossa Política de cookies .