Aeration in wastewater treatment accounts for approximately 60% of the total energy consumption in wastewater treatment plants. Energy consumption is the main cost driver in wastewater treatment, and its optimization is one if the many challenges faced by plant operators also having to meet ever more demanding safety legislation. Our online oxygen and nutrient measurement solutions not only drive energy savings in aeration control, they enable demonstrable improvements in biological processes.
Principais fatos
Up to 30%
of the energy costs
in a wastewater treatment plant can be saved by using our solution for aeration control.
Process overview
Discover the aeration process in wastewater treatment
Reliable aeration requires the accurate monitoring of the multiple environmental parameters necessary for optimal bacteriological processes, such as oxygen, ammonium, nitrate, pH, temperature and suspended solids. Such monitoring increases greatly the complexity of management of the modern wastewater treatment plant.
Our extensive portfolio of instruments, services and solution help to optimize the aeration process, enabling reliable and efficient plant management.
Discover our portfolio of liquid analysis sensor covering all important parameters
Take a closer look on our thermometers and transmitters from temperature measurement
Manage up to 8 measuring points of similar or different parameters with our multichannel transmitter Liquiline CM448. Open communication interfaces sustain system integration, smooth operations and effortless maintenance and calibration
The first step in nitrogen removal is nitrification. This requires close monitoring of the degradation of ammonium and represents a significant cost factor, as this type of liquid analysis often requires the addition of further substances to enable measurements.
Our reliable, easy to use and durable technologies for measuring ammonium concentration throughout nitrification enable the operator to react early to ammonium level disturbances.
Monitoring and sustaining the oxygen levels vital for a reliable aeration process can lead to significant energy costs for the wastewater treatment plant. Plant operators rely on fast response times and low maintenance of equipment.
Oxygen levels are controlled by comparing the measured concentration and the set-point. Our oxygen monitoring solutions can be flexibly adapted to your requirements, delivering reliable and accurate results rapidly.
Juntamente com a Endress+Hauser, a Veolia Wasser Deutschland GmbH desenvolveu uma solução para a dosagem automática e orientada à demanda por precipitantes nos reservatórios de aeração em Colditz.
A combinação da medição de oxigênio, amônia e nitrato com controle de aeração relacionado à carga pode ajudar operadores a melhorar o desempenho da fábrica.
O Liquiline Control regula a nitrificação e desnitrificação na estação de tratamento de efluentes de Stadtlohn. O sistema de controle garante conformidade com os valores de limite e otimiza o uso de energia.
Remoção automatizada do nitrogênio na Stadtlohn WWTP
Tratamento eficiente da efluentes com Oxymax COS61D no Sequencing Batch Reactor de uma empresa de laticínios
/
Takeaway
How we can help
Our advanced monitoring solutions enable optimal control of the aeration process, reducing energy and chemicals consumption whilst continuing to satisfy all current legislation.
Advanced monitoring of environmental parameters for reliable bacteriological processes
Improved nitrification process control for reduced ammonium usage
Precise oxygen measurement for optimal energy consumption of the blower
Solutions
Discover our related solutions
Remoção de fósforo de efluentes com Liquiline Control
Descubra a solução em automação de Liquiline Control para a remoção confiável de fósforo de efluentes, processos estáveis mesmo durante cargas de pico e redução de custos através do uso otimizado de precipitantes.
Além de todas as tecnologias de sistema e medição relacionadas, oferecemos também software para todos os setores da indústria que permitem aproveitar todo o potencial de seus processos de operação.
Optical analysis systems for monitoring composition and concentration in solids, liquids, slurries, particles, and gases - for laboratory, process, and emission monitoring.
Conheça nossos analisadores de gás e sistemas de medição completos que auxiliam no controle do processo e no monitoramento das emissões. O portfólio também abrange medição de partículas, soluções digitais e monitoramento de túneis.
Água, gás natural, vapor, óleo mineral e produtos químicos são alguns dos fluidos que precisam ser medidos quase diariamente. Selecione o medidor de vazão/caudal que melhor responde às necessidades do processo.
Água, bebidas, laticínios e produtos químicos ou farmacêuticos precisam ser analisados todos os dias. Escolha o dispositivo mais adequado para as necessidades de seus processos com um portfólio abrangente.
Notas finais
Related articles
Discover more interesting articles
Industrial water treatment
Effective and reliable industrial water treatment is essential for safe and efficient processes.
Industrial wastewater treatment
Optimize industrial wastewater treatment for cost effective compliance.
Wastewater sludge treatment
Optimized wastewater sludge treatment helps reduce costs, improve digester performance, and comply with environmental regulations!
Sua privacidade é muito importante
Usamos cookies para melhorar sua experiência de navegação, coletamos estatísticas para otimizar a funcionalidade do site e entregar anúncios e conteúdo personalizados.
Ao selecionar "Aceitar todos", você consente nosso uso de cookies.
Para mais detalhes, revise nossa Política de cookies .