Tente buscar por palavras-chaves, código de pedido ou produto ou número de série, por exemplo, "CM442" ou "informações técnicas"
Insira pelo menos 2 caracteres para iniciar a busca.
  • Histórico

Enhance slurry polymerization control with real-time reaction visibility

Inline Raman spectroscopy delivers continuous insight into monomer depletion, polymer growth, and hydrogen behavior in slurry reactors — for earlier decisions, more stable grades, and lower off-spec risk in polyethylene and polypropylene production.

Polymers Oy polyethylene plant, Porvoo, Finland, Borealis, chemical industry
Introduction

Protecting grade integrity in the slurry polymerization process

Polypropylene or polyethylene slurry polymerization is governed by fast, multi‑phase chemistry dynamics. Small, undetected shifts in monomer concentration, hydrogen levels, or polymer formation can propagate quickly — affecting the consistency of product properties, molecular weight targets, and reactor stability.

In real industrial environments, this risk is amplified by:

  • Opaque, high-solids slurry systems that limit conventional analytics
  • Delays between sampling, laboratory analysis, and corrective action
  • Uncertainty during grade transitions, startups, and scale-up phases

The largest material and margin losses typically occur before operators know the reaction has stabilized.

Insight

What becomes visible with inline Raman spectroscopy

Inline Raman spectroscopy embeds chemical intelligence directly inside slurry reactors, providing continuous, in‑situ visibility where traditional techniques cannot operate.

It enables real‑time access to:

  • Monomer and comonomer depletion (e.g., ethylene, propylene)
  • Polymer formation progress, even in opaque, high solids mixtures
  • Low level hydrogen concentration, critical for molecular weight and melt flow rate (MFR) control
  • Chemistry deviations as they occur, not after the batch or transition is complete

This insight is available across liquid, solid, and gas phases, and can be established within the first hour of reaction.

polyolefin, slurry polymerization output ©Endress+Hauser
Action

How reaction visibility changes operational decisions

When chemistry insight is available continuously inside the slurry polymerization reactor, decisions shift from reactive to proactive. Operators and engineers can:

  • Detect deviations while corrective action is still possible
  • Identify when a grade has reached in‑spec quality during transitions
  • Stabilize operating conditions faster after startups or restarts
  • Make scale‑up decisions based on real reaction behavior rather than indirect signals

The impact lies not in generating more data, but in enabling decision‑grade visibility at the exact moment when chemistry behavior changes.

Engineered reaction control inside the slurry reactor

In the slurry polymerization process, grade transitions and early reaction phases are where product quality and throughput are most at risk. By making monomer depletion, polymer formation, and hydrogen behavior visible directly inside the reactor and throughout the reaction, inline Raman monitoring shifts control from indirect inference to reaction‑level insight. Decisions are taken while the reaction is still controllable, and deviations are corrected before off‑spec material is produced. This removes uncertainty from the most critical production moments, stabilizes grade transitions, and enables operators to demonstrate consistent quality and higher effective throughput by design — not by post‑batch correction.

Measurable value

From transparency to measurable production impact

In slurry olefin polymerization production, a significant share of off‑spec material is generated during grade transitions, when operators wait to confirm that the new grade has reached specification. By detecting polymer formation and grade stabilization earlier, inline Raman monitoring shortens the time required to switch from off‑spec to in‑spec collection.

For slurry production of ethylene or propylene, the economic impact of reaction visibility is determined by how early operators can confidently identify grade stabilization and act on it. Each delay between actual reaction stabilization and confirmed decision‑making results in unnecessary off-spec output and lost production margin.

Example of economic impact under realistic operating conditions

Earlier reaction‑level insight during grade transitions can translate into recovered in-spec material and measurable annual value. The underlying question for each operation is not whether similar gains are possible, but how much transition time and off-spec volume could be eliminated if decisions were taken at the moment the reaction truly stabilizes.

Benefits:

  • Typical off‑spec transition time without real‑time insight: ~90 minutes
  • Off‑spec transition time with Raman‑based grade detection: ~60 minutes
  • Reduction of off‑spec output per transition: ~30 tons
  • For 3 transitions per week, this represents ~4,680 tons of recovered in‑spec material per year
  • With an illustrative price difference between in‑spec and off‑spec material of ~400 USD/ton, this corresponds to ~1.87 M USD/year potential value

In practice, the economic upside scales directly with how much earlier grade transitions can be verified and in-spec collection resumed.

This value can be realized in real slurry reactors through:

  • Immersion Raman probes installed directly in slurry reactors
  • Operation in ATEX environments, with analyzers located in controlled areas
  • Sensitivity sufficient to quantify monomers, polymers, and trace hydrogen inline
  • Phased deployment from lab → pilot → production, preserving analytical models and process understanding

Rather than replacing existing control systems, Raman technology augments them by making previously invisible reaction variables available for control, optimization, and decision‑making.

Borealis employee at polymer chemical industry plant @Borealis
Case study

Proven in an industrial slurry polymerization process

Borealis partnered with Endress+Hauser to monitor monomer depletion and polymer growth in a slurry propylene or ethylene polymerization process using inline Raman spectroscopy.

  • Real‑time monitoring across liquid, solid, and gas phases in polymerization processes
  • Quantification of propylene, polypropylene, and trace hydrogen in the polymerization process
  • Clear reaction visibility within the first hour of operation of the polymerization process
  • Increased confidence when scaling from lab-to-pilot to full production
Alexander Standler at Borealis Polyolefine

"The knowledge and know-how of Endress+Hauser to apply optical analysis in the petrochemical and polymer sectors was instrumental in improving our polymerization process development."

Alexander Standler, Expert online gas analyzer, Borealis Polyolefine GmbH, Linz, Austria
Our expertise

Why Endress+Hauser?

We help polymer manufacturers engineer safe, consistent, high‑performance production processes by delivering:

  • Proven Raman systems for ATEX environments
  • Immersion probes built for multiphase, evolving reaction conditions
  • Deep expertise in polymer chemistry and process analytics
  • Strong consultative selling, including chemometrics and experimental design
  • Extensive global service network with strong local technical support

From lab development to full‑scale production, our technology strengthens process understanding and ensures consistent polymer quality.

Operational rollout

Does Raman spectroscopy make sense for your process?

Explore practical considerations and self‑assessment questions to determine where and how Raman spectroscopy might be a good fit to deliver real value in your chemical process.

Product highlights

Explore our Raman spectroscopy systems

/
FAQ

Everything you need to know 

Next steps

Contact us

Discuss your process challenges with our chemical industry experts. We are here to support you.

Notas finais

Might also interest you