We implemented an efficient logistics concept at Brenntag Schweizerhall AG's Basel site
Chemicals distributor Brenntag Schweizerhall AG provided clear proof of their competence in the area of customer proximity through partnership: The company set up in Infrapark Baselland so that they could supply chemical raw materials directly to the businesses there.
Control cabinet with integrated operating panel
Benefits
Chemical raw materials in the required quantity and concentration "just in time"
Faster and more reliable data exchange thanks to the integration of 9 production buildings in the automation network
Complete delivery and commissioning of the entire automation technology from a single source
"Efficient automation technology is a must in order to deliver chemical raw materials just in time"
Wolfram Heymann, CEO
Brenntag Schweizerhall AG
The customer's requirements
Construction of such plants is no ordinary challenge as working with sulfuric acid, hydrochloric acid and caustic soda requires more stringent safety precautions. Therefore a risk analysis was first commissioned which would serve as the basis for the project. The project also included full automation of all processes. Brenntag Schweizerhall AG chose Endress+Hauser (Schweiz) AG as the supplier for the measurement instrumentation and automation technology.
The Endress+Hauser solution
All aspects of the automation concept had to be implemented. The task was to manage the processes reliably based on the risk analysis carried out and to design the plant in such a way that operation is easy. The plant is operated via 8 local stations as well as from Brenntag Schweizerhall AG's headquarters in Basel.
Água, gás natural, vapor, óleo mineral e produtos químicos são alguns dos fluidos que precisam ser medidos quase diariamente. Selecione o medidor de vazão/caudal que melhor responde às necessidades do processo.
Descubra as soluções industriais da Endress+Hauser para aplicações de transferência de custódia de produtos líquidos em caminhões e vagões ferroviários, com precisão e segurança.
Descubra como as soluções da Endress+Hauser aumentam o rendimento do cais e melhoram o descarregamento de líquidos de embarcações na indústria de petróleo e gás natural.
Nossos especialistas técnicos estão disponíveis para ajudá-lo.
Brenntag Schweizerhall AG
Brenntag Schweizerhall AG is the Swiss subsidiary of Brenntag AG, the global leader in the distribution of chemicals. The company has approximately 220 employees and offers its customers tailor-made logistics and service concept.
Sua privacidade é muito importante
Usamos cookies para melhorar sua experiência de navegação, coletamos estatísticas para otimizar a funcionalidade do site e entregar anúncios e conteúdo personalizados.
Ao selecionar "Aceitar todos", você consente nosso uso de cookies.
Para mais detalhes, revise nossa Política de cookies .